Use "Ctrl-F" to search for specific words in this FAQ.
| Question: Will my Optimate panel projects/software run on the EZText panels? |
| Answer: No. |
| FAQ ID: 728 |
| Question: What NEMA ratings do the EZText panels have? |
| Answer: NEMA 4 (indoor) and NEMA 4X (indoor) |
| FAQ ID: 729 |
| Question: On the EZText panels, how can I know if a message is local or from the PLC? |
| Answer: By the PLC Message LED. |
| FAQ ID: 730 |
| Question: How many set points can the EZ-SP panel have? |
| Answer: 256 |
| FAQ ID: 731 |
| Question: How many messages can the EZ-220/EZ-220L/EZ-420/EZ-220P panels have? |
| Answer: 256 |
| FAQ ID: 732 |
| Question: Can I put my own labels on the EZText panel pushbuttons? If so, how? |
| Answer: Yes! See the Help File for instructions. |
| FAQ ID: 733 |
| Question: How many comm. ports do the EZText panels have? |
| Answer: One. |
| FAQ ID: 734 |
| Question: Can PLC messages be stored/displayed in folders? |
| Answer: No. |
| FAQ ID: 735 |
| Question: Can local messages be stored/displayed in folders? |
| Answer: Yes. |
| FAQ ID: 736 |
| Question: Will the EZText panels mount in the same cutout and mounting studs as the OP panels? |
| Answer: Yes. |
| FAQ ID: 737 |
| Question: Will my EZText panel be able to talk to multiple PLCs on the same RS422 network? |
| Answer: Yes. Your addressing would be in this format. Node number then address. I.E. 2-v2000, 3-v2000,...etc. This information is also in the help file of the EZ Text edit software. |
| FAQ ID: 742 |
| Question: Does the EZ-420 have a contrast button? |
| Answer: Yes, in the setup of the panel (hardware, not software) you can select the two up/down buttons and change the contrast. |
| FAQ ID: 759 |
| Question: Can you print data from an EZText panel? |
| Answer: No. It does not support serial port printing functions. |
| FAQ ID: 764 |
| Question: Will the EZText panel work with the DL05 and DL05 networks? |
| Answer: Yes. |
| FAQ ID: 765 |
| Question: Q: Can your EZTEXT panels communicate with a Modicon PLC? |
| Answer: A: Yes, Modbus RTU |
| FAQ ID: 781 |
| Question: Q: Do the EZ Text panels support RS 485 or DH485? |
| Answer: A: No,they do NOT support RS-485 or Allen-Bradley DH-485. |
| FAQ ID: 782 |
| Question: Which versions of Entivity(ThinknDo)Live and Studio support connection to EZ Text panels? |
| Answer: EZ text panels can be connected to WinPLCs and HX-EBCs when using Live V5.5 and later and Studio V6.5 and later. |
| FAQ ID: 894 |
| Question: What type of external Power fuses are recommended for the EZTouch and EZText Panels? |
| Answer: Recommended EZText Fuse: 0.5 Amp, slo-blow Recommended EZTouch Fuse: 1.5 or 2 Amp, slo-blow |
| FAQ ID: 905 |
| Question: I just loaded a new project to my EZ Text panel and none of my Local or PLC messages work but, all other functions of the panel work fine. |
Answer:
|
| FAQ ID: 942 |
| Question: Do you have an adapter for the D2-DSCBL and EZ-2CBL cables so that I can use them on port 2 of a DL06, DL250-1, or DL260 instead of on port 1? I am using DirectSoft32 with the RJ-12 PLC connector cable (D2-DSCBL) and/or I am using an EZ-Text/EZ-Touch panel with the RJ-12 PLC connector (EZ-2CBL) to connect to port 1 of my DL06, DL250-1, or DL260 PLC. I want to connect to port 2 of these processors, which has a 15-pin high density connector. |
| Answer: Yes In any of the situations listed above, you can use the FA-15HD adapter to connect to port 2 of a DL06, DL250-1, or DL260. The FA-15HD adapter will work with DirectSoft32 and the D2-DSCBL, or with an EZ-Text or EZ-Touch panel and the EZ-2CBL cable to allow them to connect to port 2 of the DL06, DL250-1, or DL260. Since port 2 is configurable on these PLCs, you must make sure the protocol and port settings match on both devices. The FA-15HD adapter can be used with the D2-DSCBL, the EZ-2CBL, or the FA-CABKIT. The FA-15HD adapter can NOT be used with the DV-1000 or the D2-HPP. |
| FAQ ID: 1024 |