AutomationDirect Logo EZText Panels Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.

Would you prefer to narrow the list of EZText Panels FAQs? Select a category from this list:


Click here to view all EZText Panels FAQs with answers on one page.

  1. Will my Optimate panel projects/software run on the EZText panels?
  2. What NEMA ratings do the EZText panels have?
  3. On the EZText panels, how can I know if a message is local or from the PLC?
  4. How many set points can the EZ-SP panel have?
  5. How many messages can the EZ-220/EZ-220L/EZ-420/EZ-220P panels have?
  6. Can I put my own labels on the EZText panel pushbuttons? If so, how?
  7. How many comm. ports do the EZText panels have?
  8. Can PLC messages be stored/displayed in folders?
  9. Can local messages be stored/displayed in folders?
  10. Will the EZText panels mount in the same cutout and mounting studs as the OP panels?
  11. Will my EZText panel be able to talk to multiple PLCs on the same RS422 network?
  12. Does the EZ-420 have a contrast button?
  13. Can you print data from an EZText panel?
  14. Will the EZText panel work with the DL05 and DL05 networks?
  15. Q: Can your EZTEXT panels communicate with a Modicon PLC?
  16. Q: Do the EZ Text panels support RS 485 or DH485?
  17. Which versions of Entivity(ThinknDo)Live and Studio support connection to EZ Text panels?
  18. What type of external Power fuses are recommended for the EZTouch and EZText Panels?
  19. I just loaded a new project to my EZ Text panel and none of my Local or PLC messages work but, all other functions of the panel work fine.
  20. Do you have an adapter for the D2-DSCBL and EZ-2CBL cables so that I can use them on port 2 of a DL06, DL250-1, or DL260 instead of on port 1?
    I am using DirectSoft32 with the RJ-12 PLC connector cable (D2-DSCBL) and/or I am using an EZ-Text/EZ-Touch panel with the RJ-12 PLC connector (EZ-2CBL) to connect to port 1 of my DL06, DL250-1, or DL260 PLC.
    I want to connect to port 2 of these processors, which has a 15-pin high density connector.


Troubleshooting Guides