AutomationDirect Logo DL205 Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.

Would you prefer to narrow the list of DL205 FAQs? Select a category from this list:


Click here to view all DL205 FAQs with answers on one page.

  1. How can I override inputs and outputs in my DL205?
  2. How do I reset my processor back to factory defaults?
  3. When using the PID loops with my D2-250, my process variable doesn't look correct coming from my analog or temperature card. What's wrong?
  4. Why can I not get any Control Output from my PID loop?
  5. Why does my Setpoint Value change in my PID loop when I go from Manual to Auto from the PID view or ladder?
  6. Can the DL205 expand beyond the local rack?
  7. Can the DL205 communicate to the DL305 or DL405 CPU's?
  8. Which DL205 CPUs support the Power Up in Run Mode feature?
  9. Which DL205 CPUs support Manual Addressing capabilities in local bases?
  10. Which DL205 CPUs support the H2-ECOM in their base?
  11. Can the DL205 handle an encoder input and drive a stepper motor at the same time?
  12. Is the DL205 base power supply fused?
  13. I need to add another module to my DL205 9-slot base, but the rack is full. What can I do?
  14. Can the DL205 be used on a Modbus network?
  15. What is the accuracy of the PLC real-time clock?
  16. What is the manufacturer and part number for the potentiometers used in the D2-240?
  17. Is there a way to change the current count of a counter while it's counting?
  18. Is Pointer addressing prohibited for analog modules located in Remote bases?
  19. Does the DL250 bottom port (port 2) support 2 wire + ground (RS-485) networks?
  20. Where can I find information on how to connect 205 I/O to a 405 master?
  21. What is the torque specification for the terminal blocks on the 205 modules?
  22. How often should I change the backup battery?
  23. Does the DL205 series support DNP 3.0 protocol?
  24. How would we check this PLC to make sure that it is calibrated?
  25. The D2-240 has no square root?
  26. Will the DL205 series work in sub-freezing temperatures?
  27. Can the D2-CTRINT do up/down counting with a single input?
  28. How do I write ASCII code for inverter to comm port on a D2-240?
  29. Why does a timer keep counting after it reaches a setpoint?
  30. What are the ratings on the internal power supply on D2-06B-1?
  31. How many outputs on a D2-CTRINT are analog?
  32. Can I use a modem to bottom port of D2-250-1 using K-seq?
  33. What do I need to read a barcode input?
  34. Can a D2-240 do ASCII in and out?
  35. Can you use an F2-04THM and another analog module in a local DL-205 PLC system?
  36. Is the analog setup for D2-250, D2-250-1 or D2-260 pointer method the same as for D2-240?
  37. Is there a DL-305 equivalent of the D2-CTRINT?
  38. Will the H2-ECOM-F work with the D2-CTRINT?
  39. Do you offer precision resistors?
  40. Are the A NOT / B NOT functions available in the H2-CTRIO module?
  41. Can the D2-240 and D2-250 do Directnet?
  42. Is there a block-clear command for D2-240 CPU?
  43. What device can be used as master from DL205 to DL405 Slice?
  44. Using a D2-250, can you access a V memory through modbus?
  45. How do you manually address with a D2-240?
  46. Can the DL205 family communicate via Ethernet?
  47. Does the D2-Ctrint need a load when testing the Pulse Output?
  48. Why am I getting an E206 from my F2-CP128?
  49. Does the D2-Ctrint work with Think & Do?
  50. What type connectors are on the H2-ECOM?
  51. Do we have Profibus protocol in the DL205?
  52. Are the internal power supplies included on the DL205 family bases?
  53. Will F2-DEVNET support the AB PLC?
  54. Is the D2-12TR fused ?
  55. Are the DL205 bases Din rail mountable?
  56. Can you configure a D2-250-1 port for remote I/O and other protocols at the same time?
  57. Using the D2-250-1, is it possible to output a dc voltage pulse of 9 ms 13 times and a 13 ms pulse 10 times?
  58. Do we recommend a UPS for the DL205 system?
  59. Will the Dsdata server link to the H2-EBC base controller?
  60. Can you do 2 way ASCII on port 2 of the D2-250-1?
  61. Will your H2- EBC work with Labview?
  62. I forgot my PLC password, what are my options?
  63. Where can I obtain the most current firmware for my CPU?
  64. Will the F2-UNICON support the D2-240?
  65. Which WINPLC will allow me to load VB or C++ program to it?
  66. My DL205 PLC won't recognize my I/O module(s). What could be the problem?
  67. Does the H2-ECOM module have SNMP support?
  68. Is there a removable EPROM/EEPROM for the D2-250-1 or D2-260?
  69. Is there a way to change the clock & calendar in the D2-250 with a D2-HPP?
  70. Can I manually address a module in a slave rack?
  71. What is the smallest PLC that has Ethernet capability?
  72. Are the commons on D2-12TR isolated from each other?
  73. Does the 6 slot base have 2600mA and 300mA / 24VDC power supply?
  74. Do we have any examples of how to connect a D2-250-1 or D2-260 to a printer?
  75. Does your line of EBCs support thermocouple input modules?
  76. What is the output voltage of the D2-CTRINT?
  77. Will any of your Counter Cards support WINPLC?
  78. How can I get more serial ports for my WINPLC?
  79. Will the ISONET work with bottom port of the D2-240?
  80. Can you write code to a DL205 CPU without any I/O?
  81. Using my laptop, Im having trouble linking up to port 2 on the D2-240 / D2-250-1 / D2-260 PLC. Where can I start trouble-shooting?
  82. Do you have TTL level input signals on the DL205?
  83. Can the D2-CTRINT count in the negative direction?
  84. Will the D2-DCM function in an EBC base?
  85. Will a DL205 CPU lose the program if it doesn't have a battery?
  86. Can I use more than one quadrature counter on a D2-CTRINT?
  87. What fuses can I use with the D2-12TR?
  88. Does the D2-250 have ASCII in capabilities?
  89. What is the A/B switch on the D2-12TR used for?
  90. Does the D2-RMSM module consume any I/O?
  91. Can I use the D2-EE-2 to back up the user program in the DL205 series CPUs?
  92. Are there differential contacts in the D2-240?
  93. Can any ADC products communicate with Modbus Plus?
  94. How man PID loops does the D2-250-1 have?
  95. Can the D2-CTRINT control two stepper motors or only one?
  96. Will the H2-ECOM support peer-to-peer communications?
  97. Can the D2-CTRINT be manually addressed to other than X0-7 and Y0-7?
  98. Where can I find documentation on the PID functions for the D2-250 CPU?
  99. In a D2-230 what register is the count accumulated in for CTRINT?
  100. In a D2-240/250-1/260 what register is the count accumulated in for CTRINT?
  101. Is a D2-230 capable of analog inputs?
  102. Can I use a modem to top port of a D2-250-1?
  103. Is it possible to use the H0/H2/H4-ECOMS Ethernet modules with Routers on a network.
  104. What is the maximum number of H2-EBC modules that the H2-ERM can support?
  105. What is the maximum altitude that your PLC can operate?
  106. Can I control a servo motor with a DirectLOGIC PLC?
  107. I have a new F2-DEVNETS-1 module, but the Think 'N' Do ConnectivityCenter (or IOView) displays an error upon connection. What is causing this error?
  108. Do you have an adapter for the D2-DSCBL and EZ-2CBL cables so that I can use them on port 2 of a DL06, DL250-1, or DL260 instead of on port 1? I’m using DirectSoft32 with the RJ-12 PLC connector cable (D2-DSCBL) and/or I’m using an EZ-Text/EZ-Touch panel with the RJ-12 PLC connector (EZ-2CBL) to connect to port 1 of my DL06, DL250-1, or DL260 PLC. I want to connect to port 2 of these processors, which has a 15-pin high density connector.
  109. What is the format of the MRW/MRX exception buffer?
  110. Can you update firmware on a a D2-250 using port #1?
  111. What is the screw size on the 15-pin D-sub for port 2?
  112. What port is used for Modbus TCP for the ECOM100 modules?
  113. What is the SCCR rating for the DL205 PLCs?
  114. Can I change the backup battery with power applied to my DL205 CPU?


Troubleshooting Guides