DirectSOFT Programming Software
Frequently Asked Questions
Press "Ctrl-F" to search for specific words in this FAQ.
Click here
to view all DirectSOFT Programming Software FAQs with answers on one page.
- Will DirectSOFT programming software connect to the GE Series 1 CPUs?
- How do I stop my computer from accessing the floppy drive every time I start DirectSOFT32?
- When I load my program with PID loops into a new processor, my loops are not present. Why not?
- How do I cut and paste from one program to another. Every time I try, the clipboard is empty when I try to paste?
- My documentation files in DirectSOFT have been corrupted. How do I repair them?
- DirectSOFT32 installation stops shortly after entering the password key code.
- I can't get PC-R30-U to install.
- Can I use DirectSoft through my USB port?
- I don't have a CD-ROM drive in my PC; how can I install DirectSOFT32?
- Which Automationdirect.com, Koyo, TI, and GE PLCs are supported by DirectSOFT?
- Does your software access or program Allen-Bradley PLCs?
- I upgraded to the new DirectSoft, but I can't get a link to my PLC.
- Does Windows 2000 support DirectSOFT?
- With DirectSOFT, how many drums can you have active at one time?
- Can the DP software share tags with DirectSOFT?
- Is DirectSOFT tested to QS9000?
- Can you program DirectSOFT in Boolean?
- Will DirectSOFT work with a GE Series One Jr?
- Can I use "PC-Anywhere" software to run DS32 from a remote location?
- I've forgotten my CPU password. What can I do?
- How do you get the status on the ladder view?
- Does your DirectSOFT software do simulation mode?
- Will the DSdata talk OPC?
- Can the password be ALL characters?
- Can DirectSoft do rung executions one at a time?
- Will DirectSoft run on Windows NT?
- Will DirectSoft run on Windows ME?
- I only have one license. Can I uninstall on one computer then reinstall on a different one?
- Can DDE Server use SNMP protocol over Ethernet? If not, can it be modified to use SNMP as a custom solution?
- Can you change a K value of a timer in Dataview?
- Is there any way other than the compare function to align a DirectSoft project and the contents of my PLC?
- Can I run 16 bit and 32 bit on the same computer?
- With Directsoft 32, how you can assign a different path to the directory.
- What is the most common or best supported protocol using Directsoft?
- Will the SR1 PLCs communicate with Directsoft?
- How do I set the clock in DirectSoft when using a D2-240?
- The software installed but did not create a link. What do I do?
- Every time DirectSoft starts up, it takes forever to search for all of my links. How can this be avoided?
- Can I connect to and view a ladder program from a Siemens 335/37 CPU with Directsoft?
- Can 2 Directsoft licenses be installed on one computer?
- How do you change the watchdog timer?
- Do you have a version of Directsoft software that will not allow the user access to the entire program?
- Do your PLCs support Wonderware?
- Will Directsoft work without the CD in the drive?
- Does Directsoft support Omron PLCs?
- Will Directsoft support Ethernet?
- Q: Will Direct soft program a TI 435 PLC ?
- Q: In DirectSOFT how do you branch a rung?
- Q: Can LOOKOUT and DirectSOFT be open at same time?
- Q: Will a Winplc work with DirectSOFT?
- How the the DEMO version of the DirectSoft32 Programming software Different from the Puchased version?
- Where can I find more FAQs (Items not covered in this series of FAQs?
- Where can I get a DirectSOFT5 manual?
- Will DirectSoft run on Windows 7 ?
Troubleshooting Guides
|