AutomationDirect Logo C-more Micro Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all C-more Micro FAQs with answers on one page.

  1. Can the Asian character sets be used on the C-More Micro panels?
  2. Can this be used with a WinPLC?
  3. Can a C-More Micro be connected using Ethernet?
  4. Can a C-More Micro be used with a CompactLogix CPU?
  5. How can I make the PLC change the screen on the C-more Micro panel?
  6. Can you change the position of the alarm message banner?
  7. Can I reset my C-More Micro to factory defaults if I cannot access the Setup menu using F1 + F5 ?
  8. I need to use an EA-MG-SP1 adaptor to extend the distance my Cmore Micro will be from the PLC. Is there a breakout option for the communicaiton wiring?


Troubleshooting Guides