AutomationDirect Logo CLICK PLCs Frequently Asked Questions


Press "Ctrl-F" to search for specific words in this FAQ.


Click here to view all CLICK PLCs FAQs with answers on one page.

  1. Can DirectSOFT or DNLoader be used with the Click PLCs?
  2. What are the capabilities of the CLICK PLC?
  3. Does CLICK PLC support any expansion such as local expansion or remote I/O?
  4. Is there any way to add additional communications ports to a CLICK PLC?
  5. What is the SCCR rating for the CLICK PLCs?
  6. Do you have wiring digrams for use with the SureStep Drives?
  7. Can the sinking type 4 - 20mA analog output of the Click PLC be used to provide a speed reference signal for the GS series drives?
  8. What is the accuracy of the Click's Real Time Clock?
  9. Why does the Click CPU keep asking for a firmware update, or says it has no firmware, but I update the fw and it doesn't accept the update?


Troubleshooting Guides