1-PHASE Line Reactor Application Matrix

230 Volt KW 230 Volt HP Line Reactor Hitachi P/N

0.2

0.25 RL-00401 HRL010L
0.4 0.5 RL-00802 HRL050H
0.75 1 RL-00801 HRL020L
1.5 2 RL-01201 HRL030L
2.2 3 RL-01801 HRL050L

Note: These are three-phase line reactors. Only the outer two windings are used. The center winding is not connected.