AutomationDirect logoApplication Story Center


<<< Return to read applications for a different product

Motor Control Applications

Motor Control Application Listing

We'd like to show the world how you're using Automationdirect.com products. If you have a story you'd like to share, please fill out this brief form. Stories posted on our Web site will receive a $50 credit. A $500 credit will be applied to stories that are developed into full-length feature articles for publication in trade magazines. If you are interested in helping develop a story into a full-length feature article, please indicate so when you complete the application.


Application: Hitachi Drive keeps up with speedy stamping press

Products Used: Hitachi SJ100 460V Drive, CH Stack Light

Description: A Hitachi variable frequency drive was used in conjunction with a Coiltek Ultrasonic loop Control Sensor to provide precision loop control to older Perfecto and Littell decoilers. The sensor sends a 0-10 VDC signal to the drive based on the height of the material loop it sees. The drive then uses this variable signal to control the speed of the decoiler drive motor. This gives the decoiler the capabilty of following the stamping presses' speed. The use of a couple of limit switches facilitates a high loop (no feed) top stop for the press and an end of stock top stop switch. The stack light is used on the decoiler to indicate to the operator that the press is out of steel (end of stock).

Submitted by:
Thomas Dickerson (tdickerson@mii.com)
Mitek Industries Inc.

Top of Page