AutomationDirect logoApplication Story Center


<<< Return to read applications for a different product

DL305 Applications

DL305 Application Listing

We'd like to show the world how you're using Automationdirect.com products. If you have a story you'd like to share, please fill out this brief form. Stories posted on our Web site will receive a $50 credit. A $500 credit will be applied to stories that are developed into full-length feature articles for publication in trade magazines. If you are interested in helping develop a story into a full-length feature article, please indicate so when you complete the application.

 


Application: DL305 system modernizes an injection stretch-blow molding machine

Products Used: 305 family PLC w/D3-350 CPU

Description: For this application, early 80's relay logic controls were replaced on an injection stretch-blow molding machine. Additionally, cycle times and process were stabalized. The 350 is currently controlling all timing and hydraulic and pneumatic outputs for all mechanical machine functions on the four station injection stretch-blow molding machine in manual, semi-auto and full automatic. All electrical selector switches, function switches, limit switches and proximity switches are used as inputs to establish which mode it is to be run in, and when preform conditioning and blow functions are turned on and off. All told, we replaced 78 relays (using up to 8 contacts in each) and were able to add cylinder operation timers not previously installed to better control the mechanical movements. Eliminating mechanical relays also had the added benifit of speeding up dry cycle time due to the faster response time of the PLC, versus the mechanical make/break time of relays. I found the pricing of the AutomationDirect components to be lower for this application. The technical help was excellent during the debug phase of the programming and start-up. I also have the option of enhancing the operation of this machine to include functions not normally installed. I can make program changes on a laptop, idle the machine to change the logic, restart it and monitor the functions as it runs.

Submitted by:
Thomas Mihalovits (TMihalovits@rdtool.com)
R&D Tool and Engineering

Top of Page


Application: DL350 PLC and DirectTouch at the heart of an automated core cutting system

Products Used: DL350 PLC, DP-C320 touch panel, various DL305 I/O and bases

Description: The DP-C320 Touch screen coupled to a DL-350 CPU enables ease of operation and data entry on the CoreTech Inc. Model CM-11 Automatic core cutter. The CM-11 is a heavy duty, fully automated core cutting system designed for maximum productivity. True “walk away” operation requires minimum tending, frees up personnel, and delivers continuous top quality output with repeatable close tolerance cutting accuracy. Engineered for 3-shift durability, the CM-11 offers simple, quick job setup and machine changeover for flexible production versatility. To eliminate much of the apprehension and confusion associated with numerous operators CoreTech has incorporated most of the operator’s controls into the DP-C320 graphic touch panel. With the DL-350 CPU the operator can change up to 840 variables and still have room for future expansion. The DL-350 also communicates directly with the motion controller for instantaneously changing cut width on the fly.

Submitted by:
CoreTech Inc.
Easton, PA
http://www.corecutting.com

Top of Page


Application: DL340 PLC drives spikes home for Norfolk Southern railroad

Products Used: DL340 PLC, DC inputs, relay outputs

Description: A DL340-based PLC is used to handle logic operations on a railroad spike driving machine. Older machines, which used relay logic, were an electrician’s nightmare with dozens of relays and a mountain of wiring. The new control system includes three DC input modules that monitor operator inputs, limit switches, and proximity sensors. The four relay output modules power 27 hydraulic and pneumatic valves used to drive an assortment of cylinders, motors, and rotary actuators.

The machine consists of a pair of independently controlled spike drivers attached to a mobile platform. It can be run by one or two operators, with one operator for each spike driver. Before allowing the machine to move, the PLC analyzes its inputs to make sure both operators are ready. After the machine has been positioned and an operator is ready to drive a spike, he presses one button which tells the PLC to step through the spike loading process. When the spike is loaded, the operator uses a joystick to position the driver and then presses a button to lower the driver to the tie. After the spike is driven, the operator pushes another button to raise the driver, and then he is ready to move on to the next tie. In the future we plan to add an Operator Interface to ease machine tuning.

Submitted by:
Norfolk Southern Corp.
Charlotte, NC

Top of Page