|
|
|
|
|
|
FS MOVE
EXPLAINED: |
|
|
|
|
|
|
|
| The
FS Move is fully defined as "Feed to Sensor". The drive will ramp
up to velocity, and stay at that velocity until the assigned input is
triggered. When the input |
|
|
is sensed, the drive
will move accordingly so that it reaches distance DI. Depending on the
settings, the drive could continue at velocity for a noticeable length of
time, |
|
or it could start the ramp down very
quickly. It depends on the values entered for VE (Velocity), DI (Distance),
and DE (Decel). |
|
|
|
| This
is a very useful move, since the drive stays in motion until the input is
triggered. For example, if parts come
out of a machine on an irregular basis, the drive could |
|
|
run a conveyor that the
parts fall on, and once the FS command has been sent to the drive, it would
continue feeding the conveyor until a part was discharged |
|
onto the conveyor, the
part would trigger the sensor, and the drive would stop the part at distance
DI after the sensor input. So no matter when the part falls |
|
|
onto the conveyor, it
ends up at the same position. |
|
| For
another example, imagine you are printing on slightly irregular lengths of
cardboard or paper. After printing, you want to cut each sheet to make sure
they are the same length. |
|
By using the FS move,
the sensor could pick up the leading edge of each sheet, and if we had setup
our system so that the DI value was 110,000 steps, then the |
|
motor would turn 11 revs
total ( let's assume that is equivalent to 11.00 inches), and the sheet would
be properly positioned, ready to be trimmed to uniform length. |
|
|
|
|
|
|
|
Remember, the drive is an
open-loop stepper system. |
|
Even though a valid value
is entered, that doesn't mean |
|
the drive/motor can
achieve your desired move. |
|
|
|
|
|
|
|
|
|
|
|
|
|
| MD |
"Motor
Disable", always do this when changing Command Mode settings. |
|
"MD" |
|
| CM21 |
"Command Mode
21", makes sure the drive is set to Point-to-Point positioning mode. |
|
"CM21" |
|
| AC |
"Accel", sets
the accel, which will apply to the starting ramp. Both Accel and Decel are
independently adjustable, if desired. |
|
"AC2" |
|
| DE |
"Decel", sets
the decel, which would apply to both changes decel ramps. |
|
"DC2" |
|
| VE |
"Velocity",
sets the peak velocity of the move. |
|
"VE3" |
|
| EG |
"Electronic
Gearing", this is the steps per rev setting of the drive |
|
"EG1000" |
|
| ME |
"Motor Enable",
enables the motor for motion |
|
"ME" |
|
| DI |
"Distance",
this is the overall move distance |
|
"DI90000" |
|
| SA |
Saves parameters in
drive. |
|
"SA" |
|
| FS1L |
Initiates the move.
After the other settings are loaded to the drive, this is the only command
required for the drive to make the move. |
"FS1L" |
|
|
FS1L sets the drive move
(FS), and tells the drive to look at the signal at input #1 (Step terminal)
for the signal to go "low" ( On). |
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|