COMMS
Now, to the PLC and communications aspect of the new SureStep drives. We will need to use Port 2 of the DL-05, -06, the D0-DCM, 250-1, 260 and 350 cpu's, and our new Click plc. 
     These have the capability of Non-Sequence (ASCII) communications. We can also use Ports 1 and 2 of the 450 processor. We strongly recommend the use of the 06, 260 and Click
      plcs, as their advanced  ASCII instructions make the data handling much easier. Only the D0-DCM can be used for ASCII communications, the other DCM modules CANNOT be used. 
All communications will be RS-232, which means each port can only connect to one drive. However, for the D0-05 and D0-06, we can add an additional DCM module ( 1 for 05, 4 for 06)
     and each DCM could connect to one drive, potentially meaning that 5 drives could be connected to a single D0-06.
ANY and ALL motion commands / sequences should be tested first by using the SCL Terminal Utility. By stepping thru your desired operation, you can verify each that each
     step works successfully. This is how we at Tech Support will troubleshoot any problems, it will be done thru SureStep Pro and the SCL Terminal Utility.
Once this has been completed, then it is time to move to programming the PLC. There are several example programs for the Fx modes of Positioning. 
     To verify the output stringsof the PRINT / PRINTV / SEND examples, we strongly recommend the use of our programming cables and the use of a PC with a Terminal Emulator 
     such as HyperTerm (included in versions of Windows EXCEPT Vista) or RealTerm. 
     For the D0-05 and the Click, use the D2-DSCBL and for the D0-06,D0-DCM,  250/-1 and 260, use the D2-DSCBL-1.
A cable will have to be made to go from the port 2 of the PLC's to the comm port of the drive. It is possible to use either of our programming cables, the D2-DSCBL ( 05 and Click) or the 
     D2-DSCBL-1  ( 06, 250, 260) with the addition of a null modem adapter and the supplied comm cable for the drive, to make a cable to test communications to the drive.  
  Click     D0-05     D0-06, 250, 250-1, 260     350  
PORT 2 DRIVE PORT 2 DRIVE PORT 2 DRIVE PORT 2 DRIVE
Pin 3 (RX) Pin 3 ( TX ) Pin 3 (RX) Pin 3 ( TX ) Pin 2 (TX) Pin 5 ( RX ) Pin 2 (TX) Pin 5 ( RX )
Pin 4 (TX) Pin 5 ( RX ) Pin 4 (TX) Pin 5 ( RX ) Pin 3 (RX) Pin 3 ( TX ) Pin 3 (RX) Pin 3 ( TX )
Pin 1 ( 0v Gnd ) Pin 2 ( Gnd) Pin 1 ( 0v Gnd ) Pin 2 ( Gnd) Pin 7 ( 0v Gnd ) Pin 2 ( Gnd) Pin 7 ( 0v Gnd ) Pin 2 ( Gnd)
Jumper  Jumper 
Pins 4 and 5 Pins 4 and 5
together together
      450      
PORT 1 DRIVE PORT 2 DRIVE
Pin 2 (TX) Pin 5 ( RX ) Pin 3 (RX) Pin 3 ( TX )
Pin 3 (RX) Pin 3 ( TX ) Pin 4 (TX) Pin 5 ( RX )
Pin 7 ( 0v Gnd ) Pin 2 ( Gnd) Pin 1 ( 0v Gnd ) Pin 2 ( Gnd)
Jumper 
Pins 4 and 5